Solid Edge FrameworkSupport Type Library
SymbolGap Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: SymbolGap Property
Description
Sets and returns the gap between the dimension symbol and the dimension value text.
Property type
Read-write property
Syntax
Visual Basic
Public Property SymbolGap As Double
Remarks
The SymbolGap value is a ratio of dimension text height.
See Also
DimensionStyle Object
|
DimensionStyle Members
Send comments
on this topic.