Solid Edge FrameworkSupport Type Library
ViewTerminatorRatio Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: ViewTerminatorRatio Property
Description
Sets and returns the size of the terminator on the viewing and cutting plane lines.
Property type
Read-write property
Syntax
Visual Basic
Public Property ViewTerminatorRatio As Double
Remarks
This value is the ratio of dimension text height.
See Also
DimensionStyle Object
|
DimensionStyle Members
Send comments
on this topic.