Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
Dim lngIdx As Long
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create an Ellipses collection object
Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1)).Ellipses2d
'Create an Ellipse object
Set objEllipse = objEllipses.AddByCenter(xCenter:=0.04, yCenter:=0.03, xMajor:= _
0.01, yMajor:=0.01, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
' Get the Index of the Ellipse
lngIdx = objEllipse.Index
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objEllipses = Nothing
Set objEllipse = Nothing
End Sub