| Solid Edge FrameworkSupport Type Library > Ellipse2d Object : Style Property | 
| Visual Basic | 
|---|
| Public Property Style As GeometryStyle2d | 
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d Dim objEllipse1 As SolidEdgeFrameworkSupport.Ellipse2d Dim objStyle As SolidEdgeFrameworkSupport.GeometryStyle2d ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'getting the Active Sheet object Set objSheet = objDoc.ActiveSheet 'Get the Ellipses2d object Set objEllipses = objSheet.Ellipses2d 'Create an ellipse2d object Set objEllipse1 = objEllipses.AddByCenter(xCenter:=0.3, yCenter:=0.25, _ xMajor:=0.1, yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise) 'Get the Style propert Set objStyle = objEllipse1.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objEllipses = Nothing Set objEllipse1 = Nothing Set objStyle = Nothing End Sub