Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Ellipses collection object
    Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).Ellipses2d
    'Create an Ellipse object
    Set objEllipse = objEllipses.AddByCenter(xCenter:=0, yCenter:=0, xMajor:= _
                                             0.02, yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' Create a Line object to Cut the Ellipse
    Set objLine1 = objDoc.ProfileSets(1).Profiles(1).Lines2d.AddBy2Points _
                   (x1:=0, y1:=-0.01, x2:=0, y2:=0.01)
    ' Trim the Ellipse
    Call objEllipse.Trim(x:=0.1, y:=0.1, CutObj1:=objLine1)
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objEllipse = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
End Sub