Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objApplicn As SolidEdgeFramework.Application
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 180 * PI / 180
    dblFin = 230 * PI / 180
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0.02, yCenter:=0.02, _
                                             xMajoraxis:=0.03, yMajoraxis:=0.02, Ratio:=0.5, _
                                             Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    If objEllpArcs.Count <> 1 Then
        MsgBox (" AddByCenter method of EllipticalArcs2d object failed")
    End If
    ' Get the Application Property
    Set objApplicn = objEllpArc.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
    Set objApplicn = Nothing
End Sub
See Also

EllipticalArc2d Object  | EllipticalArc2d Members

Send comments on this topic.