Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objCircle As SolidEdgeFrameworkSupport.Circle2d
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim lngZOrder1 As Long
    Dim lngZOrder2 As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create an EllipticalArc object
    dblStrt = 180 * PI / 180
    dblFin = 230 * PI / 180
    Set objEllpArc = objSheet.EllipticalArcs2d.AddByCenter(xCenter:=0.25, yCenter:=0.25, _
                                                           xMajoraxis:=0.03, yMajoraxis:=0, Ratio:=0.5, _
                                                           Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Create Line and Circle objects intersecting the EllipticalArc
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.5, y2:=0.2)
    Set objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.2, y:=0.2, Radius:=0.1)
    lngZOrder1 = objEllpArc.ZOrder
    ' BringToFront the EllipticalArc object
    Call objEllpArc.BringToFront
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objEllpArc = Nothing
    Set objCircle = Nothing
    Set objLine = Nothing
End Sub