Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
Dim dblStrt As Double
Dim dblFin As Double
Dim dblMinRad As Double
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create an EllipticalArcs2d collection object
Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1)).EllipticalArcs2d
'Create an EllipticalArc object
dblStrt = 180 * PI / 180
dblFin = 230 * PI / 180
Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0, yCenter:=0, _
xMajoraxis:=0.03, yMajoraxis:=0, Ratio:=0.5, _
Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
' Get the MinorRadius of the EllipticalArc object
dblMinRad = objEllpArc.MinorRadius
objEllpArc.MinorRadius = 0.06
' USER DISPLAY
If dblMinRad <> 0.015 Or objEllpArc.MinorRadius <> 0.06 Then
MsgBox ("Error in the MinorRadius property of EllipticalArc2d object")
End If
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objEllpArcs = Nothing
Set objEllpArc = Nothing
End Sub