Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc1 As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 180 * PI / 180
    dblFin = 230 * PI / 180
    Set objEllpArc1 = objEllpArcs.AddByCenter(xCenter:=0.02, yCenter:=0.02, _
                                              xMajoraxis:=0.03, yMajoraxis:=0.02, Ratio:=0.5, _
                                              Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Mirror the EllipticalArc2d object
    Call objEllpArc1.Mirror(x1:=0.1, y1:=0, x2:=0.1, y2:=0.1)
    If objEllpArcs.Count <> 1 Then
        MsgBox (" Mirror method of EllipticalArc2d object failed")
    End If
    ' Mirror the EllipticalArc2d object
    Call objEllpArc1.Mirror(x1:=0.1, y1:=0, x2:=0.1, y2:=0.1, BooleanCopyFlag:=True)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc1 = Nothing
End Sub