Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objRelns As SolidEdgeFrameworkSupport.Relationships2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 180 * PI / 180
    dblFin = 230 * PI / 180
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0.02, yCenter:=0.02, _
                                             xMajoraxis:=0.03, yMajoraxis:=0.02, Ratio:=0.5, _
                                             Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Create an Arc object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                      objDoc.RefPlanes(1)).Arcs2d
    Call objArcs.AddByStartAlongEnd(xStart:=0.01, yStart:=0, xAlong:=-0.01, _
                                    yAlong:=-0.01, xEnd:=-0.01, yEnd:=0)
    ' Create a fillet between the Line & EllipticalArc object
    Call objArcs.AddAsFillet(Obj1:=objArcs(1), Obj2:=objEllpArc, Radius:=0.05, _
                             xDirection:=0, yDirection:=0)
    ' Get the Relationships Property
    Set objRelns = objEllpArc.Relationships
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
    Set objArcs = Nothing
    Set objRelns = Nothing
End Sub