Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
Dim objLinStyle1 As SolidEdgeFrameWork.LinearStyle
Dim objLinStyle2 As SolidEdgeFrameWork.LinearStyle
Dim objLinStyle3 As SolidEdgeFrameWork.LinearStyle
Dim dblStrt As Double
Dim dblFin As Double
Dim strStyleName As String, strStyleParent As String
Dim xStart As Double, yStart As Double, xEnd As Double, yEnd As Double
Dim x1 As Double, y1 As Double, x2 As Double, y2 As Double
Dim objStyle As Object
Dim lngIdx As Long
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
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Create an EllipticalArc object
dblStrt = 0 * PI / 180
dblFin = 90 * PI / 180
Set objEllpArc = objSheet.EllipticalArcs2d.AddByCenter(xCenter:=0.25, yCenter:=0.25, _
xMajoraxis:=0.03, yMajoraxis:=0, Ratio:=0.5, _
Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
' Create a LinearStyle2d Object
strStyleName = "LinearStyleDotted"
strStyleParent = "Dotted"
Set objLinStyle1 = objDoc.LinearStyles.Add(Name:=strStyleName, Parent:=strStyleParent)
' Get the Start point of the EllipticalArc
Call objEllpArc.GetStartPoint(x:=xStart, y:=yStart)
' Get the End point of the EllipticalArc
Call objEllpArc.GetEndPoint(x:=xEnd, y:=yEnd)
Call objEllpArc.AddSegmentedStyle(x1:=xStart, y1:=yStart, _
x2:=0.25, y2:=0.235, Style:=objLinStyle1)
' Create a LinearStyle2d Object
strStyleName = "LinearStyleDashed"
strStyleParent = "Center"
Set objLinStyle2 = objDoc.LinearStyles.Add(Name:=strStyleName, Parent:=strStyleParent)
Call objEllpArc.AddSegmentedStyle(x1:=0.22, y1:=0.25, _
x2:=xEnd, y2:=yEnd, Style:=objLinStyle2)
' Create a LinearStyle2d Object
strStyleName = "LinearStyleCenter"
strStyleParent = "Center"
Set objLinStyle3 = objDoc.LinearStyles.Add(Name:=strStyleName, Parent:=strStyleParent)
Call objEllpArc.AddSegmentedStyle(x1:=0.25, y1:=0.235, _
x2:=0.22, y2:=0.25, Style:=objLinStyle3)
' Remove All SegmentedStyles
Call objEllpArc.RemoveAllSegmentedStyles
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objEllpArc = Nothing
Set objLinStyle1 = Nothing
Set objLinStyle2 = Nothing
Set objLinStyle3 = Nothing
End Sub