Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
Dim dblStrt As Double
Dim dblFin As Double
Dim x As Double, y As Double
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create an EllipticalArcs2d collection object
Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1)).EllipticalArcs2d
'Create an EllipticalArc object
dblStrt = 180 * PI / 180
dblFin = 230 * PI / 180
Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0, yCenter:=0, _
xMajoraxis:=0.03, yMajoraxis:=0, Ratio:=0.5, _
Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
' Set the MinorAxis of the EllipticalArc object
Call objEllpArc.SetMinorAxis(x:=0, y:=0.15)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objEllpArcs = Nothing
Set objEllpArc = Nothing
End Sub