Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objL2 As SolidEdgeFrameworkSupport.Line2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 0
    dblFin = 235 * 3.14159 / 180
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0, yCenter:=0, _
                                             xMajoraxis:=0.04, yMajoraxis:=0, Ratio:=0.5, _
                                             Orientation:=1, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Create a Line object which intersects the EllipticalArc object
    Set objL1 = objDoc.ProfileSets(1).Profiles(1).Lines2d.AddBy2Points _
                (x1:=0, y1:=0, x2:=-0.1, y2:=0)
    ' Trim the EllipticalArc object
    Call objEllpArc.Trim(x:=0.1, y:=0.1, CutObj1:=objL1)
    ' Get the EndPoint of EllipticalArc object
    Dim x1 As Double, y1 As Double, x2 As Double, y2 As Double
    Call objEllpArc.GetStartPoint(x:=x1, y:=y1)
    'Call objL1.GetEndPoint(x:=x2, y:=y2)
    If (x1 <> -0.04) > 0.0001 Or Abs(y1 - 0) > 0.0001 Then
        MsgBox ("Error in the Trim method of EllipticalArc2d object")
    End If
    ' Delete the EllipticalArc & Line objects
    Call objEllpArc.Delete
    'Create an EllipticalArc object
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0, yCenter:=0, _
                                             xMajoraxis:=0.04, yMajoraxis:=0, Ratio:=0.5, _
                                             Orientation:=1, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Create 2 Line objects which intersect the EllipticalArc object
    Set objL2 = objDoc.ProfileSets(1).Profiles(1).Lines2d.AddBy2Points _
                (x1:=0, y1:=0, x2:=0, y2:=0.1)
    ' Trim the EllipticalArc object
    Call objEllpArc.Trim(x:=-0.1, y:=0.1, CutObj1:=objL2, CutObj2:=objL1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
End Sub