Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
Dim dblStart As Double, dblEnd As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create an Ellipses collection object
Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1)).Ellipses2d
'Create an Ellipse object
Set objEllipse = objEllipses.AddByCenter(xCenter:=0.04, yCenter:=0.03, _
xMajor:=0.01, yMajor:=0.01, _
Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
If objEllipses.Count <> 1 Then
MsgBox (" Error in the Ellipses2d Property of the Profile object")
End If
' Create an EllipticalArcs2d Collection object
Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1)).EllipticalArcs2d
dblStart = 45 * PI / 180
dblEnd = 235 * PI / 180
' Create an EllipticalArc2d object
Set objEllpArc = objEllpArcs.AddByStartEndEllipse(StartAngle:=dblStart, EndAngle:=dblEnd, _
Ellipse:=objEllipse)
' Call objEllipse.Delete
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objEllipses = Nothing
Set objEllipse = Nothing
Set objEllpArcs = Nothing
Set objEllpArc = Nothing
End Sub