Solid Edge FrameworkSupport Type Library
BoxAlignment Property
Description
Sets and returns the status of the alignment of a feature control frame. Note: This is a multi-level feature control option. if it's set true value, all first and second box would align and text move to the center of box.
Property type
Read-write property
Syntax
Visual Basic
Public Property BoxAlignment As Boolean
See Also

FeatureControlFrameDataSet Object  | FeatureControlFrameDataSet Members

Send comments on this topic.