| Solid Edge FrameworkSupport Type Library > FeatureControlFrames Collection : Style Property |
| Visual Basic |
|---|
Public Property Style As DimensionStyle |
Private Sub Form_Load() Dim objApp As SolidEdgeFramework.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames Dim objDimStyle As SolidEdgeFrameworkSupport.DimensionStyle Dim objDimStyle1 As SolidEdgeFrameworkSupport.DimensionStyle ' Local variables to be declared here ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If On Error GoTo 0 'Get the Active Sheet object Set objSheet = objDoc.ActiveSheet 'Get the FeatureControlFrames collection object Set objFCFs = objSheet.FeatureControlFrames 'Create a DimensionStyle object Set objDimStyle = objDoc.DimensionStyles(1) 'Assign the created DimensionStyle to the FeatureControlFrames collection object objFCFs.Style = objDimStyle 'Get the Dimension Style associated with FeatureControlFrames collection object Set objDimStyle1 = objFCFs.Style ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objFCFs = Nothing Set objDimStyle = Nothing Set objDimStyle1 = Nothing End Sub