Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame
' Local variables to be declared here
Dim lngZorder As Long
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
On Error GoTo 0
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Get the FeatureControlFrames collection object
Set objFCFs = objSheet.FeatureControlFrames
'Add a new FeatureControlFrame
Set objFCF = objFCFs.Add(x:=0.1, y:=0.1, z:=0)
objFCF.PrimaryFrame = "FLVB0.001MCVBA"
Call objFCF.AddVertex(x:=0.2, y:=0.2, z:=0)
objFCF.BreakLine = True
'Draw line over the FeatureControlFrame
Call objSheet.Lines2d.AddBy2Points(x1:=0.125, y1:=0.1, x2:=0.275, y2:=0.25)
Call objSheet.Lines2d.AddBy2Points(x1:=0.2, y1:=0.25, x2:=0.3, y2:=0.125)
'Get the Zorder of the FeatureControlFrame
lngZorder = objFCF.ZOrder
'Place the FCF infornt of Line
Call objFCF.BringForward
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objFCFs = Nothing
Set objFCF = Nothing
End Sub