Solid Edge FrameworkSupport Type Library
GetFreeSpacePoint Method
The coordinates of the free space point.
The coordinates of the free space point.
The coordinates of the free space point.
Description
Returns the coordinates of the terminal connect point for a leader line that belongs to the active dimensioning object.
Syntax
Visual Basic
Public Sub GetFreeSpacePoint( _
   ByRef x As Double, _
   ByRef y As Double, _
   ByRef z As Double _
) 
Parameters
x
The coordinates of the free space point.
y
The coordinates of the free space point.
z
The coordinates of the free space point.
Remarks
The z argument applies only to 3-D objects.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame
    ' Local variables to be declared here
    Dim dblX As Double, dblY As Double, dblZ As Double
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Add a new FeatureControlFrame
    Set objFCF = objFCFs.Add(x:=0.1, y:=0.1, z:=0)
    objFCF.PrimaryFrame = "FLVB0.001MCVBA"
    'Get the point at which the FeatureControlFrame is placed
    objFCF.GetFreeSpacePoint x:=dblX, y:=dblY, z:=dblZ
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
    Set objFCF = Nothing
End Sub
See Also

FeatureControlFrame Object  | FeatureControlFrame Members

Send comments on this topic.