Solid Edge FrameworkSupport Type Library
RotationAngle Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
FeatureControlFrame Object
: RotationAngle Property
Description
Sets and returns the angle, in radians, at which the object is rotated along its major axis.
Property type
Read-write property
Syntax
Visual Basic
Public Property RotationAngle As Double
See Also
FeatureControlFrame Object
|
FeatureControlFrame Members
Send comments
on this topic.