Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame
' Local variables to be declared here
Dim dblVertices(5) As Double
Dim lngVertexCount As Long
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
On Error GoTo 0
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Get the FeatureControlFrames collection object
Set objFCFs = objSheet.FeatureControlFrames
'Add a new FeatureControlFrame
Set objFCF = objFCFs.Add(x:=0.125, y:=0.1, z:=0)
objFCF.PrimaryFrame = "FLVB0.001MCVBA"
'Add few vertices to the FeatureControlFrame
Call objFCF.AddVertex(x:=0.2, y:=0.2, z:=0)
Call objFCF.AddVertex(0.25, 0.225, 0)
objFCF.BreakLine = True
dblVertices(0) = 0.1: dblVertices(1) = 0.1 'First vertex co-ords
dblVertices(2) = 0.15: dblVertices(3) = 0.125 'Second vertex co-ords
dblVertices(4) = 0.2: dblVertices(5) = 0.175 'Third vertex co-ords
Call objFCF.SetVertices(VertexCount:=2, Vertices:=dblVertices)
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objFCFs = Nothing
Set objFCF = Nothing
End Sub