| Solid Edge FrameworkSupport Type Library > FeatureControlFrame Object : Style Property |
| Visual Basic |
|---|
Public Property Style As DimStyle |
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame Dim objFCFStyle As SolidEdgeFrameworkSupport.DimStyle ' Local variables to be declared here ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If On Error GoTo 0 'Get the Active Sheet object Set objSheet = objDoc.ActiveSheet 'Get the FeatureControlFrames collection object Set objFCFs = objSheet.FeatureControlFrames 'Add a new FeatureControlFrame Set objFCF = objFCFs.Add(x:=0.1, y:=0.1, z:=0) objFCF.PrimaryFrame = "FLVB0.001MCVBA" Call objFCF.AddVertex(x:=0.2, y:=0.2, z:=0) objFCF.BreakLine = True 'Get the DimStyle associated with the FCF Set objFCFStyle = objFCF.Style ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objFCFs = Nothing Set objFCF = Nothing Set objFCFStyle = Nothing End Sub