Solid Edge FrameworkSupport Type Library
Frame Object Members
Overview 
Public Properties
Public Property BorderColorSets and returns the color of the border when the BorderVisible property is True.
Public Property BorderDashTypeNameSets and returns the line style to use for the border of the referenced frame object.
Public Property BorderPrintedSpecifies whether or not the border of the referenced frame object is to be printed when the container is printed.
Public Property BorderVisibleSpecifies whether or not the border of the referenced frame object is visible.
Public Property BorderWidthSets and returns the width of the line used to draw the border of the referenced frame object.
Public Property MarginSets and returns the minimum distance from the extents of the OLE object to the extents of the frame boundary.
Public Property ShapeOptionSets and returns the shape for the border of the referenced object.
See Also

Frame Object

Send comments on this topic.