Solid Edge FrameworkSupport Type Library
GeometryStyle2d Object Members
Overview 
Public Methods
Public Method GetDashGapReturns the dash and gap characteristics of the referenced style object.
Public Method SetDashGapDefines the dash and gap characteristics of a linear element.
Public Method UseActiveStyleAssigns the current active linear style to the referenced graphic object.
Public Properties
Public Property AutoPhaseIf True, specifies that the negative dash gaps for the referenced style object are automatically extended based on the size of the edge.
Public Property DashGapCountReturns the number of dashes and gaps in the dash definition.
Public Property DashNameSets and returns the named dash style for the referenced object.
Public Property DashStrokePercentSets or returns the percentage of the first dash in the first stroke that needs to be drawn.
Public Property LinearColorSets and returns the group edge color for the referenced style object.
Public Property LinearNameSets and returns the linear style for the referenced object.
Public Property UnitsSets and returns the units in which the line width is defined.
Public Property WidthReturns the width of the referenced object.
See Also

GeometryStyle2d Object

Send comments on this topic.