Solid Edge FrameworkSupport Type Library
AddGostWeldSymbol Method
Description
Creates a GostWeldSymbol. For creating PMI GostWeldSymbol a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of GostWeldSymbol.
Syntax
Visual Basic
Public Function AddGostWeldSymbol( _
   ByVal AnnotInitData As AnnotInitData _
) As GostWeldSymbol
Parameters
AnnotInitData
See Also

GostWeldSymbols Collection  | GostWeldSymbols Members  | Solid Edge ST5 - What's New

Send comments on this topic.