Solid Edge FrameworkSupport Type Library
BreakLineDirection Property
Description
Sets and returns the direction (left or right) in which the break line runs along the x axis.
Property type
Read-write property
Syntax
Visual Basic
Public Property BreakLineDirection As Boolean
See Also

GostWeldSymbol Object  | GostWeldSymbol Members  | Solid Edge ST3 - What's New

Send comments on this topic.