Solid Edge FrameworkSupport Type Library
Angle Property
Description
The angular rotation of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Angle As Double
Remarks
For Rectangles, this value represents the rotation of the entire object. The angle is represented in Radians.
See Also

Image2d Object  | Image2d Members

Send comments on this topic.