Solid Edge FrameworkSupport Type Library
FlipHorizontal Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Image2d Object
: FlipHorizontal Property
Description
This read-write Boolean property flips the horizontal orientation of the referenced Image2d object.
Property type
Read-write property
Syntax
Visual Basic
Public Property FlipHorizontal As Boolean
Remarks
When this property is True, the horizontal orientation is flipped; when False, it is not.
See Also
Image2d Object
|
Image2d Members
Send comments
on this topic.