Solid Edge FrameworkSupport Type Library
FlipVertical Property
Description
This read-write Boolean property flips the vertical orientation of the referenced Image2d object.
Property type
Read-write property
Syntax
Visual Basic
Public Property FlipVertical As Boolean
Remarks
When this property is True, the vertical orientation is flipped; when False, it is not.
See Also

Image2d Object  | Image2d Members

Send comments on this topic.