Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objTextBox As SolidEdgeFrameworkSupport.TextBox
    Dim objLeaders As SolidEdgeFrameworkSupport.Leaders
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create a text Box in the active sheet.
    Set objTextBox = objSheet.TextBoxes.AddByHtWdAng(x1:=0.1, y1:=0.1, z1:=0, ht:=0.1, wd:=0.15, ang:=0)
    'Add some text to the Text
    objTextBox.Text = "THIS IS FOR TESTING ONLY"
    'Create Leaders collection object
    Set objLeaders = objSheet.Leaders
    'Create a leader attatched to text box
    Call objLeaders.AddByTerminator(TerminatorObject:=objTextBox, x1:=0.125, _
                                    y1:=0.2, z1:=0, Keypoint1:=True, _
                                    x2:=0.2, y2:=0.4, z2:=0)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objTextBox = Nothing
    Set objLeaders = Nothing
End Sub