Specifies the annotation object to which the leader is to be connected.
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
Specifies whether the object or a key point of the terminator object is to be used. If True, the leader's terminal end is placed with respect to the TerminatorObject; if False, the nearest key point on that object is selected.
Description
Specifies a new object and/or connect point for the terminal end of an annotatino object's leader.
Syntax
Visual Basic
Public Sub SetTerminator( _
ByVal TerminatorObj As Object, _
ByVal x As Double, _
ByVal y As Double, _
ByVal z As Double, _
ByVal keyPoint As Boolean _
)
Parameters
TerminatorObj
Specifies the annotation object to which the leader is to be connected.
x
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
y
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
z
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
keyPoint
Specifies whether the object or a key point of the terminator object is to be used. If True, the leader's terminal end is placed with respect to the TerminatorObject; if False, the nearest key point on that object is selected.
Remarks
If the annotation object is placed with respect to a key point, the point of reference is the key point.