Solid Edge FrameworkSupport Type Library
Document Property
Description
Returns the document to which the referenced object belongs.
Property type
Read-only property
Syntax
Visual Basic
Public Property Document As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objDocmnt As SolidEdgePart.PartDocument
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) _
                   .Lines2d
    ' Create a Line2d object
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0.1)
    ' Get the Document Property
    Set objDocmnt = objLine1.Document
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
    Set objDocmnt = Nothing
End Sub
See Also

Line2d Object  | Line2d Members

Send comments on this topic.