Solid Edge FrameworkSupport Type Library
Extend Method
Double that specifies the coordinates of the point at which the referenced element is to be extended.
Double that specifies the coordinates of the point at which the referenced element is to be extended.
The object to which the referenced element is to extend.
Description
Extends open graphic elements to a specified location.
Syntax
Visual Basic
Public Sub Extend( _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal TargetObj As Object _
) 
Parameters
x
Double that specifies the coordinates of the point at which the referenced element is to be extended.
y
Double that specifies the coordinates of the point at which the referenced element is to be extended.
TargetObj
The object to which the referenced element is to extend.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) _
                   .Lines2d
    ' Create 2 Line2d objects
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    Set objLine2 = objLines.AddBy2Points(x1:=0.05, y1:=0.1, x2:=0.05, y2:=0.15)
    ' Extend Line2 to meet Line1
    Call objLine2.Extend(x:=0.02, y:=0.1, TargetObj:=objLine1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
End Sub
See Also

Line2d Object  | Line2d Members

Send comments on this topic.