Solid Edge FrameworkSupport Type Library
GetStartPoint Method
Coordinates of the start point.
Coordinates of the start point.
Description
Returns the coordinates of the start point for the referenced object.
Syntax
Visual Basic
Public Sub GetStartPoint( _
   ByRef x As Double, _
   ByRef y As Double _
) 
Parameters
x
Coordinates of the start point.
y
Coordinates of the start point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim x As Double
    Dim y As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                       objDoc.RefPlanes(1)).Lines2d
    ' Create a Line2d object
    Set objLine1 = objLines.AddBy2Points(x1:=-0.01, y1:=0, x2:=0.01, y2:=0.01)
    'Get the StartPoint of the Line object
    Call objLine1.GetStartPoint(x:=x, y:=y)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
End Sub
See Also

Line2d Object  | Line2d Members

Send comments on this topic.