Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
Dim objAttributeSets As Object
Dim bAttribSetPresent As Boolean
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
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
On Error GoTo 0
'Create an empty Lines2d collection object
Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) _
.Lines2d
' Create a Line2d object
Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0.1)
' Get the AttributeSets collection object
Set objAttributeSets = objLine1.AttributeSets
'Create an AttributeSet
Call objAttributeSets.Add("MyAttribSet")
'Check for the presence of created Attributeset
bAttribSetPresent = objLine1.IsAttributeSetPresent("MyAttribSet")
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objLines = Nothing
Set objLine1 = Nothing
Set objAttributeSets = Nothing
End Sub