Solid Edge FrameworkSupport Type Library
IsChamfer Property
Description
Specifies whether or not the referenced Line2d object is a chamfer.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsChamfer As Boolean
Remarks
If a Line2d object is created with the AddAsChamfer method, the line may be a chamfer. This means that the line has chamfer relationships to two other lines. The IsChamfer property tests the Line2d object to determine if it is a chamfer. Use the Chamfer property to access the ChamferGeometry2d object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine3 As SolidEdgeFrameworkSupport.Line2d
    Dim bChamfer As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Lines2d
    ' Create 2 Line2d objects
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    Set objLine2 = objLines.AddBy2Points(x1:=0.1, y1:=0, x2:=0.1, y2:=0.1)
    ' Create another Line object using the AddAsChamfer Method
    Set objLine3 = objLines.AddAsChamfer(Obj1:=objLine1, Obj2:=objLine2, xDirection:=1, _
                                         yDirection:=1, SetBackA:=0.04, SetBackB:=0.03)
    bChamfer = objLine3.IsChamfer
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
    Set objLine3 = Nothing
End Sub
See Also

Line2d Object  | Line2d Members

Send comments on this topic.