Solid Edge FrameworkSupport Type Library
Mirror Method
Specifies the x coordinate of the first point on the mirror axis.
Specifies the y coordinate of the first point on the mirror axis.
Specifies the x coordinate of the second point on the mirror axis.
Specifies the y coordinate of the second point on the mirror axis.
Specifies whether or not the copied object will be active.
Description
Copies the referenced object about an axis.
Syntax
Visual Basic
Public Function Mirror( _
   ByVal x1 As Double, _
   ByVal y1 As Double, _
   ByVal x2 As Double, _
   ByVal y2 As Double, _
   Optional ByVal BooleanCopyFlag As Variant _
) As Object
Parameters
x1
Specifies the x coordinate of the first point on the mirror axis.
y1
Specifies the y coordinate of the first point on the mirror axis.
x2
Specifies the x coordinate of the second point on the mirror axis.
y2
Specifies the y coordinate of the second point on the mirror axis.
BooleanCopyFlag
Specifies whether or not the copied object will be active.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) _
                   .Lines2d
    ' Create a Line2d object
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0.1)
    ' Make a MirrorCopy of the object
    Call objLine1.Mirror(x1:=-0.1, y1:=0.1, x2:=0.1, y2:=0.1)
    If objLines.Count <> 1 Then
        MsgBox ("Error in the Mirror Method of Line2d Object")
    End If
    Call objLine1.Delete
    'Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) _
                   .Lines2d
    ' Create a Line2d object
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0.1)
    ' Make a MirrorCopy of the object
    Call objLine1.Mirror(x1:=-0.1, y1:=0.1, x2:=0.1, y2:=0.1, BooleanCopyFlag:=True)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
End Sub
See Also

Line2d Object  | Line2d Members

Send comments on this topic.