Solid Edge FrameworkSupport Type Library
ProjectionDashName Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Line2d Object
: ProjectionDashName Property
Description
When Projection is set to True, this read-write String property specifies the style name for the referenced Line2d object. If ProjectionDashName is not a valid style name, the dot style is used.
Property type
Read-write property
Syntax
Visual Basic
Public Property ProjectionDashName As String
See Also
Line2d Object
|
Line2d Members
Send comments
on this topic.