Solid Edge FrameworkSupport Type Library
Select Method
Description
Selects the referenced object in the active window.
Syntax
Visual Basic
Public Sub Select() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create Lines collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                       objDoc.RefPlanes(1)).Lines2d
    'Create a Line object
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    ' Select the Line object
    ' Set objLine2 = objLine1.Select
    Call objLine1.Select
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
End Sub
See Also

Line2d Object  | Line2d Members

Send comments on this topic.