Solid Edge FrameworkSupport Type Library
SetKeyPoint Method
Specifies the index of the key point/handle.
Specifies the x coordinate of the specified key point.
Specifies the y coordinate of the specified key point.
Specifies the z coordinate of the specified key point.
Description
Sets the position for a specified key point.
Syntax
Visual Basic
Public Sub SetKeyPoint( _
   ByVal Index As Long, _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double _
) 
Parameters
Index
Specifies the index of the key point/handle.
x
Specifies the x coordinate of the specified key point.
y
Specifies the y coordinate of the specified key point.
z
Specifies the z coordinate of the specified key point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim x As Double
    Dim y As Double
    Dim z As Double
    Dim KeyPtType As KeyPointType
    Dim HType As HandleType
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) _
                   .Lines2d
    ' Create a Line2d object
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    'Set the KeyPoint(endpoint) of the Line object
    Call objLine1.SetKeyPoint(Index:=2, x:=0.02, y:=0, z:=0)
    'Get the KeyPoint(endpoint) of the Line object
    Call objLine1.GetKeyPoint(Index:=2, x:=x, y:=y, z:=z, KeyPointType:= _
                              KeyPtType, HandleType:=HType)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
End Sub
See Also

Line2d Object  | Line2d Members

Send comments on this topic.