| Solid Edge FrameworkSupport Type Library > Line2d Object : Style Property |
| Visual Basic |
|---|
Public Property Style As GeometryStyle2d |
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objLines2d As SolidEdgeFrameworkSupport.Lines2d Dim objLine1 As SolidEdgeFrameworkSupport.Line2d Dim objStyle As SolidEdgeFrameworkSupport.GeometryStyle2d ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'getting the Active Sheet object Set objSheet = objDoc.ActiveSheet ' getting the lines2d collection object Set objLines2d = objSheet.Lines2d ' Create Line2d object using AddBy2Points method Set objLine1 = objLines2d.AddBy2Points(x1:=0.05, y1:=0.05, x2:=0.1, y2:=0.05) 'get style of line2d Set objStyle = objLine1.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objLines2d = Nothing Set objLine1 = Nothing Set objStyle = Nothing End Sub