Solid Edge FrameworkSupport Type Library
RemoveAllSegmentedStyles Method
Description
Removes all segments defined for the referenced graphic object.
Syntax
Visual Basic
Public Sub RemoveAllSegmentedStyles() 
Remarks
Removing segmented styles does not remove the geometry. Instead, it removes the linear styles applied to the graphic object defined by the segments. If a segment is blank (for example, when the linear style is null), it reappears when its segment is removed.
See Also

LineString2d Object  | LineString2d Members

Send comments on this topic.