Solid Edge FrameworkSupport Type Library
RemoveAllSegmentedStyles Method
Description
Removes all segments defined for the referenced graphic object.
Syntax
Visual Basic
Public Sub RemoveAllSegmentedStyles() 
Remarks
Removing segmented styles does not remove the geometry. Instead, it removes the linear styles applied to the graphic object defined by the segments. If a segment is blank (for example, when the linear style is null), it reappears when its segment is removed.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet





    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
End Sub
See Also

Point2d Object  | Point2d Members

Send comments on this topic.