| Solid Edge FrameworkSupport Type Library > Point2d Object : Style Property | 
| Visual Basic | 
|---|
| Public Property Style As GeometryStyle2d | 
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objPoints As solidedgeframeworksupport.Points2d Dim objPoint As solidedgeframeworksupport.Point2d Dim objPointStyle As Object ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'getting the Active Sheet object Set objSheet = objDoc.ActiveSheet 'Create Points collection Set objPoints = objSheet.Points2d 'Create a Point Set objPoint = objPoints.Add(x:=0.2, y:=0.2) 'get Style Set objPointStyle = objPoint.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objPoints = Nothing Set objPoint = Nothing End Sub