Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfile As SolidEdgePart.Profile
Dim objRPattern As SolidEdgeFrameworkSupport.RectangularPattern2d
Dim lngOffsetType As SolidEdgeConstants.PatternOffsetTypeConstants
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Create a new Profile object
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1))
' Create a RectangularPattern2d object on the profile
Set objRPattern = objProfile.RectangularPatterns2d.Add(OriginX:=0, OriginY:=0, _
Width:=0.1, Height:=0.05, Angle:=0, OffsetType:=sePatternFixedOffset, _
XCount:=6, YCount:=4, XSpace:=0.015, YSpace:=0.01)
' Get and change the type of the Offset for the RectangularPattern2d object
lngOffsetType = objRPattern.OffsetType
objRPattern.OffsetType = sePatternFillOffset
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfile = Nothing
Set objRPattern = Nothing
End Sub