Solid Edge FrameworkSupport Type Library
GetRelatedObjectCount Method
Returns the number of objects associated with the relation.
Description
Returns the number of objects to that are associated with the referenced Relation2d object.
Syntax
Visual Basic
Public Sub GetRelatedObjectCount( _
   ByRef Count As Long _
) 
Parameters
Count
Returns the number of objects associated with the relation.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objCirc2 As SolidEdgeFrameworkSupport.Circle2d
    Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
    Dim objReln1 As SolidEdgeFrameworkSupport.Relation2d
    Dim objProfile As SolidEdgePart.Profile
    Dim lngCnt As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create 2 Circle objects
    Set objCirc1 = objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.1)
    Set objCirc2 = objProfile.Circles2d.AddByCenterRadius(x:=0.05, y:=0.05, Radius:=0.12)
    ' Create a Concentric Relation between the objects
    Set objRelns = objProfile.Relations2d
    Set objReln1 = objRelns.AddConcentric(Object1:=objCirc1, Object2:=objCirc2)
    ' Get the No. of Related objects
    Call objReln1.GetRelatedObjectCount(Count:=lngCnt)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCirc1 = Nothing
    Set objCirc2 = Nothing
    Set objRelns = Nothing
    Set objProfile = Nothing
    Set objReln1 = Nothing
End Sub
See Also

Relation2d Object  | Relation2d Members

Send comments on this topic.