Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
Dim objCirc2 As SolidEdgeFrameworkSupport.Circle2d
Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
Dim objReln1 As SolidEdgeFrameworkSupport.Relation2d
Dim objProfile As SolidEdgePart.Profile
Dim objAttributeSets As Object
' Local variables to be declared here
Dim bAttribSetPresent As Boolean
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
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
On Error GoTo 0
' Create an empty Profile
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1))
' Create 2 Circle objects
Set objCirc1 = objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.1)
Set objCirc2 = objProfile.Circles2d.AddByCenterRadius(x:=0.05, y:=0.05, Radius:=0.12)
' Create a Concentric Relation between the objects
Set objRelns = objProfile.Relations2d
Set objReln1 = objRelns.AddConcentric(Object1:=objCirc1, Object2:=objCirc2)
' Get the AttributeSets collection object
Set objAttributeSets = objReln1.AttributeSets
'Create an AttributeSet
Call objAttributeSets.Add("MyAttribSet")
'Check for the presence of created Attributeset
bAttribSetPresent = objReln1.IsAttributeSetPresent("MyAttribSet")
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objCirc1 = Nothing
Set objCirc2 = Nothing
Set objRelns = Nothing
Set objProfile = Nothing
Set objReln1 = Nothing
Set objAttributeSets = Nothing
End Sub