Solid Edge FrameworkSupport Type Library
Parent Property
Description
Returns the parent object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Parent As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine3 As SolidEdgeFrameworkSupport.Line2d
    Dim objRelns As SolidEdgeFrameworkSupport.Relationships2d
    Dim objParent As SolidEdgeFrameworkSupport.Line2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an empty Lines2d collection object
    Set objLines = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                       objDoc.RefPlanes(1)).Lines2d
    ' Create 2 Line2d objects
    Set objLine1 = objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    Set objLine2 = objLines.AddBy2Points(x1:=0.1, y1:=0, x2:=0.1, y2:=0.1)
    ' Create another Line object using the AddAsChamfer Method
    Set objLine3 = objLines.AddAsChamfer(Obj1:=objLine1, Obj2:=objLine2, xDirection:=1, _
                                         yDirection:=1, SetBackA:=0.04, SetBackB:=0.03)
    ' Get the Relationships of the Line object
    Set objRelns = objLine3.Relationships
    ' Get the Parent Property
    Set objParent = objRelns.Parent
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
    Set objLine3 = Nothing
    Set objRelns = Nothing
    Set objParent = Nothing
End Sub
See Also

Relationships2d Collection  | Relationships2d Members

Send comments on this topic.