Solid Edge FrameworkSupport Type Library
CropTop Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SmartFrame2dDefaults Object
: CropTop Property
Description
Sets and returns the distance from the origin of the referenced object to the top of the frame or view.
Property type
Read-write property
Syntax
Visual Basic
Public Property CropTop As Double
Remarks
Specified in container units
See Also
SmartFrame2dDefaults Object
|
SmartFrame2dDefaults Members
Send comments
on this topic.