Solid Edge FrameworkSupport Type Library
Rotation Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SmartFrame2dDefaults Object
: Rotation Property
Description
For OLE objects, specifies the angle at which the object is rotated along its major axis. For hatch lines, sets and returns the rotation angle used to display hatch lines.
Property type
Read-write property
Syntax
Visual Basic
Public Property Rotation As Double
See Also
SmartFrame2dDefaults Object
|
SmartFrame2dDefaults Members
Send comments
on this topic.