Solid Edge FrameworkSupport Type Library
ScaleFactor Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SmartFrame2dDefaults Object
: ScaleFactor Property
Description
Sets and returns the scale factor between an object and its source document.
Property type
Read-write property
Syntax
Visual Basic
Public Property ScaleFactor As Double
Remarks
This property sets and returns the paper-to-model scale as a factor.
See Also
SmartFrame2dDefaults Object
|
SmartFrame2dDefaults Members
Send comments
on this topic.